I’ve been working on this PCB (in EAGLE) since September, and I’m glad it’s finally almost done. Since I have no formal training in electronics though, I must admit I’m pretty much shooting blindly with my ground planes, stitching, and capacitors. I’f you’ve got the time, I’d really appreciate some feedback on how my ground plane and via stitching looks and how it can be improved, and definitely comment on other things if you can, because it can only help me improve. ![]()
Also, I’ve only got 7 caps going from +5V to ground. (1x100uF polarized cap, and 6x0.01uF ceramics) Do I need more, or to change their values? The board has two ATmega328s on it, and some LCD circuitry that hits about 1.5MHz tops.
Here are a couple of nice big screenshots:
http://img29.imageshack.us/img29/2722/lcd10.png
http://img139.imageshack.us/img139/7734/lcd2.png
If you need more information, files, etc. and want to help with more detail, please PM me. ![]()
Thanks for the help, I totally appreciate it!