I have a SARA-R5 Asset Tracker that needs the SARA-R5 chip reset. It connects to the network when a SIM is in place (the blue light comes on around 20 seconds after power on). I get GPS data when I run Arduino Apps. But under M-Center I can’t get the SARA chip to return OK after any commands. It is running old firmware (2.06) so maybe I need to reflash it anyway?
I just realized the Update PCB needs to be in the MicroMod slot for M-Center to work. Processor boards route the USB to themselves instead of the SARA-R5. M-Center will not work with a processor board in the MicroMod slot. All is well ![]()