Is there any trick to getting the NEO-M9N to communicate on the RX/TX data lines? I have the same MEGA 2560 board loaded with the same software I’ve used on various NEO M6 derivatives and all I did was add a level shifter on the RX/TX lines. I’m powering the board with the 3.3V supply from the MEGA. Same data wires other than the level shifter. I plug in the NEO 6 and all is well. I plug in the NEO 9 and I get no data. I’ve tried reversing the TX/RX wires but no change. I see that the UART shares the SPI lines but the documentation says, if I short the SPI jumper it disables the UART. Is this correct. The jumpers are open as shipped from SparkFun.
I would post pics of the setup but I don’t have a camera right now available.