NEO F10N Data Logging and RINEX Conversion

I recently acquired the sparkfun NEO-F10N in hopes of conducting studies using the L1 and L5 bands. While the unit seems to work fine, I found that I am unable to convert the recorded ubx file into RINEX observation data. I know from previous experience with u-blox products that this is related to the UBX-RXM-RAWX message.

Is there a special firmware that allows the logging of rawx messages to be enabled? Or perhaps a workaround that allows for RINEX observation files to be generated? Any help in regards to how I can acquire the raw GNSS data would be great.

Hi Moe (@MN-16 ),

Sorry, the NEO-F10N does not support the UBX-RXM-RAWX message. It’s only available on u-blox High Precision (HPG) GNSS modules. The NEO-F10N is Standard Precision (SPG). Our cheapest HPG boards are probably the NEO-M8P (L1) followed by the NEO-F9P (L1/L5).

We’ve also had good results from the LG290P, but there you need to configure it to output RTCM which can be converted to RINEX.

I hope this helps,
Paul

As I recollect, earlier samples had it enabled, now it’s available from uBlox as an Option via NEO-F10N-00B-20

Oh i see, thanks for this. That explains why uBlox lists the F10N as a product with carrier phase output. Its a shame they opted to remove the RAWX feature, would’ve made for a wonderfully cost effective solution for L1/L5.

I’m guessing theres also no alternative firmware or possible add-on either that would allow for this?

Thanks! Is it already standard for uBlox to only provide RAWX on HPG units? Or are there SPG options exempt to this?

That used to be the case… Although, going back a few years, the NEO-M8T (timing variant) did output RAWX and was significantly cheaper than the NEO-M8P.

I wasn’t aware of that new NEO-F10N -20 variant. Thanks @clive1 !

We only carry the standard non -20 variant… And I’m not seeing any -20 stock at any of the usual suppliers. Perhaps it is currently only available direct from u-blox?