Hello - I (think I) need to create a new Device, a TI UA78M12CKVURG3 (http://www.ti.com/lit/ds/symlink/ua78m12.pdf), which is a 12V fixed voltage regulator; I need the SOT223 package. If it is possible, I could use the V_REG_78XX Symbol (78XX), and the SOT223 Package, both from Sparkfun’s library. How do I marry them up in a new Device, including connecting 4 pads to three pins? Further complicating things is the fact that I’m on a Macbook, and I don’t yet habla Apple.
Thanks a million,
DeanB
(NuB to Eagle, Sparkfun, electronics in general, Mac - but having fun!)