New Serial Graphic LCD 128x64 Arduino Library

Hello.

I’m new to microcontrollers and bought [this product to start off with something easy. After a few days of trail and error I looked at the comments on the product page and realized that the firmware was kinda buggy. I also noticed that someone had written a new firmware for the backpack, so i went ahead and flashed it. This really solved everything, contrast isn’t changing, backlight isn’t flickering, write speed was fixed and i have seen no more strange symbols appearing when writing commands to it.

I could not find a library for it so I decided to try and write one myself with a little help from iklln6’s code from the comments.

So here it is: [serialGLCD library for Arduino

This firmware and library also adds more functionality like drawing bitmaps, filled boxes and 2 fonts!

As far as i can tell this works perfectly with [This firmware

(Note that this firmware ONLY works with the 128x64 display!)

I have not commented the library itself, but I included an example sketch with comments

Please have a look at the library and tell me if something could have been done another way…

And Sparkfun: please fix the firmware!

EDIT: Project was moved to SourceForge](SerialGLCD download | SourceForge.net)](serialGLCD library for Arduino download | SourceForge.net)](http://www.sparkfun.com/products/9351)