Hi folks,
I just want to confirm, I assume I CANNOT use a non-I2C board with QWIIC sensors, correct?
Recently ordered the QWIIC log writer and pulse oximetry sensors, had planned on using them with my ESP32 Thing that I’ve had in my parts case for awhile. They’re both red, right? Should work!
Initially assumed that the QWIIC system was more about simple stuff like connections and jacks, I’d be able to wire the ESP32 Thing to it with just a little more work than plugging in the wire. After a bit of reading that I should’ve done first, turns out it’s a whole different bus, it sounds FAR different than TX/RX.
My project will use the oximetry and heart rate sensor and record values to the micro-SD card. The wifi capability of that board would let me get the time from a network time server. Coulda bought the non-QWIIC logger, but that sensor seems to be QWIIC-only.
Bonus points will be awarded if you can give me a good QWIIC board that’ll let me do the same wifi stuff. I think the SparkFun Thing Plus - ESP32 WROOM (U.FL) is my best bet yeah? Kinda like the design of the SparkFun Redboard Edge, but would have to add wifi and a logger to it somehow.
Thanks!