No data from DAN-F10N

Hi Sparkfun,

I got a brand-new DAN-F10N breakout board - but cannot get any data from it.
It is connected to a Windows computer, and recognised as CH340 chip on COM7.
However - u-center 2 software cannot find a bitrate to “talk” to it, neither I can do manually.
In addition - no LEDs seem to light up when the board is connected.
I’ve checked the software and USB by connecting a similar board with other UBLOX chip - it was recognised right away and worked.

Please advise - are there any bridges etc to make the board work with USB?

Thanks,
Dmitry

I haven’t used this particular gps so i don’t know if there are anything you need to do to get data flowing. Usually they just work. Sounds like you might have a dud?

Hi Dmitry - Welcome! There is a power LED on the board that should illuminate when connected. If that’s not turning on, double check that other devices (your phone, etc) correctly connect over the USB C cable you are using and work on the computer port you’re connecting to.

Hello and thanks for a quick response.
I did some measurements and found that either the power stabiliser U3 is faulty - since with present Vin and EN the 3.3 V line shows 0.11 V - or the line itself is pulled down by the faulty part.
This is pretty much aligned with what I see on the computer - it sees CH340 which is powered by 5V, but cannot communicate with the GPS module behind it.

Was it purchased from us? If so head over to Returns - SparkFun Electronics (contact vendor if purchased elsewhere) and we’ll get ya squared away

Hi TS-Russell,

I got it via the distributor, will contact them ASAP.
Thanks for a quick response!

Best regards,
Dmitry

1 Like

I came for the forum exactly for this problem. I can confirm that the board works with external FTDI connected to serial bypassing onboard serial adapter.

I have no easy option to return the two board that I have which both shows the same problem. Any suggestion regarding this problem? Surely I can utilize the boards with external serial adapters but the whole selling point for those boards were to easy connection to a mobile phone through USB. Is it possible or meaningful for me to chance the chip on the the board? Any known compatible chip?

I had a bit different problem - in my case the GPS chip wasn’t getting power.
Got the board replaced via the distributor.

With regard to your question - the schematics is available here and all chips are named.