I purchased a “Force Sensitive Resistor - Long” and it’s been working great until today. My project could no longer read it, and when checked with a multimeter directly no reading is made (as if disconnected). Visually both the strip itself and pins look fine.
I carefully soldered on some wires to connect to some female headers on my project (partly because of the negative reviews of that product). However, I have since disconnected it and am testing the strip’s pins directly with a multimeter like when I was first testing it. I attached a picture (shows both sides). Thanks!
The solder could be the issue here. Did you by chance rework those solder connections prior to the FSR malfunctioning? It is difficult to see in your photos but it looks like there is solder going all the way up the plated connector pins on the bottom of the FSR. Comparing your photos to the ones on the [product page shows the difference.
It is a bit hard to tell in the picture, but I read the concerns so only applied solider at the thinner ends of the metal tabs. I also only soldiered/used heat once. It was working great for a few weeks, then (like I said) stopped giving any resistance readings. Thanks for the help so far, btw!
Have you tested for resistance on the substrate material instead of on the pins/wires? It is rare for these to suddenly stop working so I am curious if there is a break going on somewhere between where you are measuring and the substrate material on the FSR.