Edited by moderator to add code tags
Compiling gcc ../src/tf_accelerometer/lis2dh12_reg.c
 Linking gcc bin/example1_edge_test.axf
 Copying gcc bin/example1_edge_test.bin...
../../../../../tools/apollo3_scripts/create_cust_image_blob.py --bin bin/example1_edge_test.bin --load-address 0xC000 --magic-num 0xCB -o bin/main_nonsecure_ota --version 0x0
Header Size =  0x80
original app_size  0x460c ( 17932 )
load_address  0xc000 ( 49152 )
app_size  0x460c ( 17932 )
w0 = 0xcb00468c
Security Value  0x10
w2 =  0x10008080
addrWord =  0xc000
versionKeyWord =  0x0
child0/feature =  0xffffffff
child1 =  0xffffffff
crc =   0x37c5774
Writing to file  bin/main_nonsecure_ota.bin
../../../../../tools/apollo3_scripts/create_cust_wireupdate_blob.py --load-address 0x20000 --bin bin/main_nonsecure_ota.bin -i 6 -o bin/main_nonsecure_wire --options 0x1
Header Size =  0x60
app_size  0x468c ( 18060 )
Writing to file  bin/main_nonsecure_wire.bin
Image from  0x0  to  0x468c  will be loaded at 0x20000
../../../bsp/tools/uart_wired_update_sparkfun.py -b 115200 COM13 -r 1 -f bin/main_nonsecure_wire.bin -i 6
Connecting with Corvette over serial port COM13...
Sending Hello.
No response for command 0x00000000
Traceback (most recent call last):
  File "C:\AmbiqSuite-Rel2.0.0\boards\SparkFun_edge_BSP-master\bsp\tools\uart_wired_update_sparkfun.py", line 341, in <module>
    main()
  File "C:\AmbiqSuite-Rel2.0.0\boards\SparkFun_edge_BSP-master\bsp\tools\uart_wired_update_sparkfun.py", line 42, in main
    connect_device(ser)
  File "C:\AmbiqSuite-Rel2.0.0\boards\SparkFun_edge_BSP-master\bsp\tools\uart_wired_update_sparkfun.py", line 61, in connect_device
    response = send_command(hello, 88, ser)
  File "C:\AmbiqSuite-Rel2.0.0\boards\SparkFun_edge_BSP-master\bsp\tools\uart_wired_update_sparkfun.py", line 238, in send_command
    raise NoResponseError
__main__.NoResponseError
make: *** [Makefile:197: bootload] Error 1