nRF2401 Directly to Sensor?

Is it possible to transmit potentiometer readings wirelessly using a either an xbee or nRF2401 with no microcontroller?

I am a programmer, but a beginner with Arduino. If anybody could point me in the right direcitons it would be very helpful.

The nRF2401 won’t work without an MCU. I wouldn’t bother with it, anyway, it’s obsolete. I’ve used the current nRF24L01+ with a PIC.

The issue here is that there are some very unforgiving size constraints. If I were to use an xbee instead, is it possible to transmit potentiometer readings without a micro controller? How could this be accomplished? Is there another transmitter that is smaller in size that could accomplish this? I only require about 30 foot range.

It should be possible to get an nRF24L01+ and an MCU into a very small volume.

You may not be aware of just how tiny microcontrollers can be. The ATtiny10 is a little less than 2 by 3 mm in the SOT-23 package, and if you can fit the code into 1kbyte, you get a happy little computer complete with an 8-bit ADC to digitize your potentiometer data. Sparkfun sells the [Nordic Fob if you’d like to see an example using a slightly larger Atmel microcontroller.](Nordic FOB - WRL-08602 - SparkFun Electronics)

If I were to use an xbee instead, is it possible to transmit potentiometer readings without a micro controller?

Yes, XBees have a few Analog (ADC) inputs. Check the XBee Documents on their Pin outs.

Note: The Series 1 XBees require an external ADC voltage reference.

vvortex3:
Is it possible to transmit potentiometer readings wirelessly using a either an xbee or nRF2401 with no microcontroller?

I am a programmer, but a beginner with Arduino. If anybody could point me in the right direcitons it would be very helpful.

You can instead nRF2401 by nRF24LE1 or other which consists the 51 MCU, no other external MCU is needed.