Hello,
I have 2 nRF24L01 ev kit and I program them via the C2 interface.
The application is very simple:
-
the first module reads the potentiometer value (every 60 ms) and sends it out continuously as 2 byte payload .
-
the second module only receives the data and acknowledges when data are received correctly.
The application works fine if I keep the TX module in run debugging mode (via C2 interface) (no breakpoints enabled).
When I disconnect the debugging cable and switch the TX module on, the RF module doesn’t enable IRQ signal anymore (therefore it’s like if it doesn’t send data).
I checked the duration of the IRQ signal when it is enable (down to zero):
in the TX module dt = 2us
in the RX module dt = 10us
Is this normal?
Have you experienced same problems with the mentioned ev kits?
Thank you,
Kind regards,
Sveva