I just got a pair of nRF24L01 modules from sparkfun. These modules are pretty cool with the exception that the output power and sensitivity is on the low side. It would be nice if a module was available with a RF amplifier plus an antenna switch. The nordic has enough channels to make it FCC legal with frequency hopping.
No, I don’t like AT style interfaces. Yes, I do want the 2mbps speed of the nordic. Yes, I like the low cost.
mzoran:
I just got a pair of nRF24L01 modules from sparkfun. These modules are pretty cool with the exception that the output power and sensitivity is on the low side. It would be nice if a module was available with a RF amplifier plus an antenna switch. The nordic has enough channels to make it FCC legal with frequency hopping.
No, I don’t like AT style interfaces. Yes, I do want the 2mbps speed of the nordic. Yes, I like the low cost.
Is this even possible? I mean, all the amplification circuitry is inside the chip, and the RX/TX mixing/switching is inside as well! If it had an external RX/TX switch like I've seen in other places than sure, it seems like you could put your amp in between the nRF24L01 and the switch. But otherwise, how would you do it?
Note that this is much more of a question than a statement… I am RF handicapped - it’s all black magic to me.