So, I’ve been using my pair of Facet’s to survey/measure property lines in rural Texas. Cell coverage is very spotty, but I’ve managed to use one Facet as a NTRIP client on a PPP-processed +_2mm ground reference point I defined. I’m getting a large error in my measurements vs the 2 paper surveys I have in hand. >2 foot difference over 1200’ marked distance from Facet vs professional survey distance.
The setup looks like this:
Facet PPP NTRIP server -->wifi to house -->WIRELESS internet service provider ( I think their tower is ~5 miles away but they’re based near Dallas 80 miles away) → Internet → EMLID NTRIP service → Internet -->Cell tower–>my iPhone as a hot spot → Android device using SW Maps bluetooth’d to Facet NTRIP client.
Physically, the two Facets are never more than 3/4 mile from one another. Electronic communication-wise, though, that’s a lot of hops, distance travelled via radios, and distance via wires and fiber. So how does this relate to the recommendation for the NTRIP client being placed 6 miles from the server? Is this where my error is coming from?
I’m going to try measuring with the Facets using radio. This is less than ideal, because I the devices can’t reach each other through the woods. My idea is to create multiple PPP locations and move around that way due to the radio los limitations.
Thoughts?