I am attempting to get my RTK Facet to utilize correction data from an NTRIP server. Thanks to help on this forum I’ve gotten the Facet to accept NTRIP data and enter the correct mode.
Since there is no station local to me I would like to setup a Base Station myself and I’ve been unsuccessfully trying to follow the instructions located on the tutorial
https://learn.sparkfun.com/tutorials/ho … tation/all
I run into two issues, my correction data is either inaccurate or the CSRS immediately kicks back an error.
The data I have been able to submit shows
The estimated coordinates ITRF14 2022-10-26 for the COM7_221026_221346.obs RINEX file are as follows:
Latitude N40° 39’ 30.5461" ± 0.478 m (95%)
Longitude W74° 28’ 14.7017" ± 0.564 m (95%)
Ellipsoidal Height 53.428 m ± 1.107 m (95%)
Orthometric Height CGVD2013 CGG2013a 87.3130 m
[40.65848502,-74.47075048,53.428]
UTM Zone 18 (North)
Northing 4500981.419 m
Easting 544739.744 m
Scale factor (point) 0.99962464
Scale factor (combined) 0.99961626
[4500981.419,544739.744,53.428]
Cartesian coordinates
X 1297267.618 ± 0.647 m (95%)
Y -4668539.782 ± 0.910 m (95%)
Z 4133761.330 ± 0.725 m (95%)
[1297267.618,-4668539.782,4133761.330]
Orbits and Clocks Used: NRCan Rapid
GNSS Data: GPS
GRS80 ellipsoid used for (x,y,z) to (lat,lon,h) transformation
The example shows getting a location less then 0.006m and I am easily 100x that. I tried two separate times with two sets of data. The data was collected with a GPS RTK2 from Sparkfun, the two datasets were both little over 28 hrs long and both had equally meh results.
I’m not sure where to start, but some things seemed odd and I am not sure if they are relevant.
When I have UBlox open and observing the data it shows 28 more satellites, however when I plot the data after capture using RTKLIB and RTKCONV is shows less then 10. I’ve attached two images showing what I see in UCenter and RTKPLOT.
So to try and rule out my setup I attempted to utilize the Facet itself to collect the data. I can’t use it as my base station and rover simultaneously, but wanted to see if I could collect good data from the Facet and get a precise measurement from that device instead (this would have hopefully ruled out bad cables, poor antenna, or other hardware problems). With the Facet, I can’t seem to get good data at all. I’ve tried varying some settings and resetting to factory, but in every case when I convert the UBX file to OBS and submit it to the CSRS PPP portal I get and error like the following.
COM9___9600_221029_011041B.obs Error : The RINEX file contains formatting errors in the observations at epoch 2022 10 29 1 11 29.99. Please correct and resubmit.
The data itself looks fine to me, I can plot position, number of satellites and it plays back just fine in UCenter. I’ve tried taking multiple data sets and they all receive the same error.
I’ve tried to put relevant information into this post, but I am sure that more information would be required so let me know what else if anything I should post up and I will do so.
Thank you very much,
Jim