Hey guys,
I been trying to pick out an LCD and the uLCD (and ezlcd but that one is TOO expensive) has caught my attention. The uLCD, or microLCD, has a bunch of neat features and has 1MB of flash which can be used to store images. It also has a lot of wonderful abilities (such as draw line, box, dot, draw image, animate images, etc). However, the LCD costs about $76 and is a bit expensive.
I was wondering if anyone knows of any LCDs that are similar but not as expensive. My current requirements are:
Less than 1.6" in height
Less than 4" in width
Color & Graphic
Touchscreen is a plus
Can be controlled by a micro w/ Rx/Tx communication or I2C (Planning to use a PIC18F series micro)
I saw the 20$ Sony LCD but that one is rather big. Do the OLED and knock-off LCDs SF carry have similar abilities?
After looking at pictures of the uLCD-OLED it seems to me it uses the same OLED screen as the one sold by SF. Is it just me or is it true?
Also, as far as I understand all you need for a “smart” LCD is an LCD, a LCD driver which takes incoming commands and does whatever with them to generate the picture on the screen and some memory to save images onto. Is this correct? How hard would it be to make your own?
Thanks in advance,
-roboude666