Hi all, I use an jtagkey like tool with openocd 0.4.0 to connect the omap3530 board,
the configuration file is the original omap3530.cfg,
the jtag board does not have srst.
In the telnet windows, if I run the “halt” command, it can’t return to the prompt again, it seems to be blocked.
If I run the “reset” command, the openocd exit.
Can any body give me some advices?
The output of openocd is:
Open On-Chip Debugger 0.4.0 (2010-08-25-15:23)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.berlios.de/doc/doxygen/bugs.html
Warn : omap3530.dsp: huge IR length 38
RCLK - adaptive
Info : device: 4 “2232C”
Info : deviceID: 341266712
Info : SerialNumber: FTTKZ0Y8A
Info : Description: USB<=>JTAG&RS232 A
Info : RCLK (adaptive clock speed) not supported - fallback to 1000 kHz
Info : JTAG tap: omap3530.jrc tap/device found: 0x0b7ae02f (mfg: 0x017, part: 0xb7ae, ver: 0x0)
Info : JTAG tap: omap3530.dap enabled
Info : omap3530.cpu: hardware has 6 breakpoints, 2 watchpoints
Error: JTAG-DP STICKY ERROR
Error: MEM_AP_CSW 0x2800042, MEM_AP_TAR 0x54011140
Error: JTAG-DP STICKY ERROR
Error: MEM_AP_CSW 0x2800042, MEM_AP_TAR 0x54011140
Error: JTAG-DP STICKY ERROR
Error: MEM_AP_CSW 0x2800042, MEM_AP_TAR 0x54011140
Error: JTAG-DP STICKY ERROR
Error: MEM_AP_CSW 0x2800042, MEM_AP_TAR 0x54011140
Error: JTAG-DP STICKY ERROR
Error: MEM_AP_CSW 0x2800042, MEM_AP_TAR 0x54011150
Error: JTAG-DP STICKY ERROR
Error: MEM_AP_CSW 0x2800042, MEM_AP_TAR 0x54011150
Error: JTAG-DP STICKY ERROR
Error: MEM_AP_CSW 0x2800042, MEM_AP_TAR 0x540111c0
Error: JTAG-DP STICKY ERROR
Error: MEM_AP_CSW 0x2800042, MEM_AP_TAR 0x540111c0