Openlog Artemis Support for AS7331 Spectral UV Sensor

There appear to be no products sold on SparkFun or elsewhere that use the visible light sensors supported by OLA. In any case, I also wanted UV and the multi-band UV of the AS7331 is very appealing. Is there anyone supporting this sensor or plans to do so?

I should point out that I’m willing to add code. I looked at the instructions at the OLA “adding sensors” page https://github.com/sparkfun/OpenLog_Art … SENSORS.md; however, the repo for making updates has no place for sensor library to go – at least I didn’t find one.

The sensor has an Arduino library for the AS7331 https://github.com/sparkfun/SparkFun_AS … no_Library

The OLA is a much better solution than the one I made with an Arduino UNO and a data logger shield back in 2012 or so.