I am curious if it is possible to have the OLA act as a thumb drive when connected to a laptop. I have an use where this would be preferable to transferring files over via packet transfer. This was a great feature in the Logomatic product and would be nice to have if possible in the OLA.
The files on the SD card can also be accessed via the USB terminal interface. A new configuration menu allows you to: list the files on the card delete individual files type the contents of an individual file to the terminal send / copy an individual file to the serial TX pin transfer individual or all files using the MODEM protocol