I am using the Sparkfun OpenLog Artemis. I have the onbard realtime battery installed. When I powered the board with an external power supply, sometime, the board won’t boot into datalogging. It kind of stuck there and draws about 10mA current. This never happened before without the onboard button battery installed. It looks the system won’t wake up from sleep.
I should have probed the reset signals etc. Before that, I just ask around here. Also, the board has no designators on silkscreen. Does anyone have an assembly drawing or something similar? It’s not easy to locate components on the board. Thanks.