I have 2 Sparkfun OpenLog units both of which act the same way. They are connected to GPSs through the UART connection, 5 Volts. One uses a Sparkfun NEO-M9N and the other is connected to an M8N. The baud rate is set correctly in the config file on the SD card.
On startup one of 4 things happens, seemingly each about 25% of the time.
-
The logger records a blank file
-
It records a file that starts with “
˜ø˜`fffà† ˜à† ˜à† xà†ff†žþž€˜” -
It records a file that starts with “顠悘晦蘘頀ᣠ砘蛠晦ᢆ鸆黾ڀ惦頀ᢞ”
-
It records a file with the correct NMEA text output.
What can I do to help the situation?
Thanks!