I’m getting ready to put in a order of pcbs to goldphoenix using the 155 square inch 2 layer special deal. I want to put three separate small boards in the same order, which apparently requires that I panelize them. These are the guidelines from their website.
- Multi-Project Panel. When the designs on the panel are different extra fees will be charged for multi-project panel. Regulations for multi-project panel are below:
Panelization of the multi-project panel must be done at customer side. We do not offer service to panelize multi-project panel.
We can also separate the multi-project panel if the number of different projects on the panel is less than six, otherwise de-panelization must be done at customer side.
If all designs on the panel are square and the same size, V score can be applied to the panel and number of
project is 20.
Only two different projects are allowed for 4 layers multi-project panel.
To order multi-project panel, customer must allow 15% fail rate for the small unite on the panel.
I really don’t even know what panelizing entails. I have the three boards in separate eagle cad files. Do I have to merge them all on to one layout, then send that to them? I’m really not sure what to do.