Philba:
I wouldn’t try to cut a populated board at all. best to get it v-scored before populating.
That is not a good view on cutting boards when you are assembling them for other people. When a person sends 100 boards, the time it takes to unload and reload the Pick and Place is wasted time. Also reflowing is more difficult. It would be easy to loose track of a board, when you have 100-10,000 separate boards in a job. Also if the boards are 0.5 x 2 inches…the chances of dropping one are greater.
All SMT assembly services attempt to populate panels (arrays) before they are cut. It saves time and labor cost.
As long as the panel is not flexed when separating, no harm can come of the components. Even v-scored boards are separated after population unless a component over hangs the cut. Most of the time it will be the last thing to be placed on the board (after separation). The separation method is by a “Depanelizer” which uses the v-score as a squeeze line. It breaks the remaining fibers holding the boards together. It is almost a shear, but uses two wheels that come together.
Population after separation increases the turn around time of a job about 40%. This is due to time taken loading and unloading the machinery.
This is the standard in the industry. You can ask any assembly house (that is doing it with automated machinery) and they will tell you it would cost much more to populate the boards independently. This does of course depend on the board size. If the board is 10 inches x 13 inches, they are not likely to be in an array (or panelized).
Separation after population is the industry norm,
James L
EDIT: Just for information, I included this website for a depaneler. It tells how close to a component it can cut. https://www.manncorp.com/depanelers/sdm … ?auto=done