Not sure where you’re headed with this one, but I’ve see this vendor ship boards with ‘vcuts’. Basically, top and bottom of the board get a heavy score line on each side. You just bend/flex the board at the score lines and you get nice, clean break.
I edited the topic a bit to match the question/answer a bit better.
The PCB page can be confusing. The minimum amount you can order is obviously 1"x1" or 1 square inch at $2.50. Your board size can actually be anything smaller than this. We will cut to your board. If you need one or two units, no problem. If you need 45 pcs at 0.3x0.4" then we may have to have a talk. Most likely we would need to get you an entire v-scored panel.
Hi there, I’m Pete. I’ve recently been hired on at Spark Fun. Nathan’s asked me to address this briefly…
We’re hesitant to do this (the whole hole thing) for fear of accidentally overlapping some holes. When that happens, bits break and the manufacturer gets irate at us. To keep costs low, there are just a few rules we like to follow, and this is one of them.