PCA9306 Level Translator horizontal pin spacing not of grid?

While I wait for my PCA9306 Level Translators to arrive, I want to prepare my circuit board. From the reviews, I understand that these customers found the vertical pin spacing to be the standard 0.1”. But they found the horizontal pin spacing non-standard. I took a screen print of the PC9306, and it is clearly not 0.7” between columns of pins. It might be 0.65”. Does anyone know? Or has Sparkfun corrected this error?

Thanks,

Rick

It’s still a thing, but we have a short photo demo of the fix PCA9306 Logic Level Translator Hookup Guide (v2) - SparkFun Learn

Thanks for the info. I looked at that picture but it didn’t register!

Hopefully Sparkfun won’t make this mistake in the future.

Can they at least add a bullet item on page 1 saying that the column spacing is 0.65” and not 0.7” rather than only implying it in a figure?

Rick