Hey folks,
My name is Steve Rosenow and I was referred here by a member of a car forum.
Before I begin with my question, I have a little background on my project.
I own a Meade LX-3/2080 Schmidt-Cassegrain telescope - with a servo motor/worm gear-driven drive base that dates back to the mid-1980s. These telescopes upon their introduction in 1985 were considered the “cream of the crop” and were the first large-scale deep-sky astrophotography platform available to the mass consumer market. As part of the telescope package, Meade offered users - as an optional accessory - a manually-driven motor drive corrector which allowed the user to completely control the tracking rate ensuring the ability of exposures longer than five minutes. These drive corrector hand controllers, known as the Meade #36 Drive Corrector, were produced in a limited quantity until the end of the LX-3 production run in 1990. Over 10,000 LX-3 telescopes were produced in 8 and 10-inch optics, with less than around a thousand hand controllers. Today, these hand controllers are either failing due to aging electronics, or are becoming extremely hard to source.
Since I am an astrophotographer who actually enjoys these older units, I would like the ability to keep control of my telescope’s tracking rate to ensure I can do exposures longer than five minutes (to eliminate horizontal star trailing due to drive error and to bring out the fainter deep sky objects).
To that end, I have sourced the original Meade wiring/component schematic from an astronomy website, plus a photo illustrating the original hand controller.
[Meade LX3/2080 handbox by [Loowit Imaging - Steve Rosenow, Photographer, on Flickr
This is a photo of what the finished product looked like. The rough size is about two inches wide or so, a little over five and a half inches long with a depth of an inch and a half.
[LX3Paddle by [Loowit Imaging - Steve Rosenow, Photographer, on Flickr
In light of that, the N/S/E/W buttons are SPDT momentary pushbuttons in a normally-closed circuit. The slight problem in faithfully recreating this controller is that the hardware Meade used (namely, the buttons) is long since out of stock. No supplier I have checked with supplies these buttons. As a result, I am having to use SPDT momentary buttons from Radio Shack (link here: http://www.radioshack.com/product/index … Id=2062541). These switches are vastly different compared to the original switch buttons Meade used.
As for the “QUARTZ/MANUAL” slider switch, it is a DPDT slider (although I have been told that a SPDT slider or toggle will work). The power cord is a six-strand coil cable terminating at a large 6-pin DIN plug.
Using the schematics, I have produced a basic idea of what I hope to achieve, which is a rectangular hand box controller very similar to the Meade original, with a toggle and the adjustment dial for solar/lunar/sidereal tracking speed. From the outside, the layout will be identical.
The main question, is that I am for the most part stuck. How would I go about creating the PCB for this?
Many thanks in advance for any assistance I can get. I have been wracking my brain for a few weeks on it.](About Steven Rosenow | Flickr)](LX3Paddle | Steven Rosenow | Flickr)](LX3Paddle | Steven Rosenow | Flickr)](About Steven Rosenow | Flickr)](Meade LX3/2080 handbox | Steven Rosenow | Flickr)](Meade LX3/2080 handbox | Steven Rosenow | Flickr)
<LINK_TEXT text=“http://farm9.staticflickr.com/8042/8010 … e179_b.jpg”>http://farm9.staticflickr.com/8042/8010422173_ef906fe179_b.jpg</LINK_TEXT>
<LINK_TEXT text=“http://farm9.staticflickr.com/8451/8042 … 4ac3_o.jpg”>http://farm9.staticflickr.com/8451/8042698852_99df614ac3_o.jpg</LINK_TEXT>
<LINK_TEXT text=“http://farm9.staticflickr.com/8032/8046 … 3275_c.jpg”>http://farm9.staticflickr.com/8032/8046460157_e65efb3275_c.jpg</LINK_TEXT>