Greetings,
I’ve just completed construction of a project using a
PCB fabbed by BatchPCB. Unfortunately there was a
via to pad short that took a bit of detective work to
find. Apart from being under the body of a component
it was so thin that a 10x eye loupe was required to
see it. A brush with a sharp knife took care of it!
Has anyone else seen PCB defects like this?
The board was the first I’ve done with EAGLE 5.0,
which I upgraded to EAGLE 5.1 during the project.
I see that EAGLE 5.2 has been released, in part
to address a known bug that causes random shorts
in the Gerber output files (!!?).
In my case I have build two identical PCBs, and
as luck would have it the first I powered up had the
short, the other does not. I can’t find any defects
in the EAGLE files, and strongly suspect this is a
random PCB fab process error (dust, dirt, or
abrasive scratch on the tooling is my likely guess).
This is the first and only BatchPCB defect I’ve found
in over a dozen board designs, but it does come on the
heels of the recent EAGLE bug fix. Which is very good
for a “no touch” fab service.
Comments Welcome!