Performance of cache in AT91RM9200

Hi everybody,

I’m doing image processing project on the AT91RM9200, so I want to increase performance by enabling the cache and the MMU. Here is the code:

void init_TLB() {

uint i, j, a; uint tlb = (uint)0x20000000;

for (i=0; i<4096; ++i) {

tlb = 0x12 | (i << 20);
}
for (i=512; i<528; ++i) {
tlb |= 0xC; // enable write_back cache for SDRAM
}
i = 0x20000000;
asm (“mcr p15, 0, %0, c2, c2, 0” : : “r”(i)); // set TLB base
i = 3;
asm (“mcr p15, 0, %0, c3, c0, 0” : : “r”(i)); // set domain access
i = 0;
asm (“mcr p15, 0, %0, c7, c7, 0” : : “r”(i)); // invalidate ICache & DCache
i = 0xC000107D;
asm (“mcr p15, 0, %0, c1, c0, 0” : : “r”(i)); // enable MMU & ICache & DCache & asyn clock
}
Then I measure the performance by counting the number of svd decompositions of a 6x6 matrix in 2.5s.
a = AT91C_BASE_ST->ST_CRTR + 5;
i = 0;
while (a > AT91C_BASE_ST->ST_CRTR) {
Q = V;
svd(Q, W, E);
++i;
}
std::cout << “\nsvd of Q\n” << W << “\nCalculated " << i << " times in 2.5s”;
I get following results:
no cache 33 times
only instruction cache 270
data and instruction cache 35
Why is it so slow when both caches are enabled? It so slow as with no cache.
Does anyone have similar experience?
Thanks