I’m in the process of Installing the Remote Camera Web Interface Software on the kit’s Pi Zero.
When I get to the point where I attempt to access the Remote Camera Web Interface Software by entering the command:
“./install.sh”
I get the following message:
WARNING: The following packages cannot be authenticated! dialog E: There are problems and -y was used without --force-yes
Any ideas and thanks?
George S.
Got past that problem by starting from scratch but hit another wall.
One I entered a username and password in the Configure Option window for the camera and select “OK” to install software I hit an error “unable to locate package PHP7.3” and the I get droped back to the system command line interface.
Again any ideas how best to proceed. I have started from scratch two time and hit this same issue.
Thanks
George S.
Make sure you are using an up-to-date version of Raspbian.
The source code for the camera web interface is hosted [here on GitHub. The is a link to the [Wiki that has installation istructions. I loaded it recently on the new Buster image and had no issues.](RPi-Cam-Web-Interface - eLinux.org)](GitHub - silvanmelchior/RPi_Cam_Web_Interface: A web interface for the RPi Cam)