Pixhawk4 board not giving +5v to the UART ports

Hi,

I’ve been working on a drone project using Pixhawk4 as the fcu, but recently I’ve started encountering this issue where half of the ports have stopped working (I have checked ports Telem2, GPS and UART/I2C port were not functioning).

When a sensor or GPS is connected to these ports, the sensors are not powering up and also not receiving/transferring any data. I am sure the sensors and the GPS module is not faulty as it is working on other Pixhawk4 board.

Weirdly, while further diagnosing I found that that the GPS, telem2 and UART ports are not receiving +5V, when I checked with with a multi-meter.

Even after removing the GPS unit (or other sensors) individually the ports are not working.

I currently have the Pixhawk4 FCU powered by the PM07 PDB, and other modules include benewake tfmini at telem2, holybro GPS to GPS port, px4flow sensor to I2C, holybro telemetry to telem1, and rc receiver to the PPM port.

Thanks

Maybe there’s a short in your wiring somewhere? If you disconnect everything from the flight controller, does 5V come back?

Hi YellowDog,

Even after disconnecting everything from the fcu, the 5V does not come.

Sounds like you might have burnt something out, it’s possible there might be a fuse inside the board that can be replaced.

Might be worth checking on the manufacturers forum to see if it’s repairable by the end user or if it needs sent back.

https://discuss.px4.io/c/pixhawk/22

Hi YellowDog,

Oh okay, it was manufactured by sparkfun itself, but I’ll try posting in the px4 forum as well.

Thanks

Hi suraj_iTron.

SparkFun carries the Pixhawk, but we don’t manufacture it. We do hope the manufacturer is able to help you with an easy fix on their forum though!

Hi TS_Chris,

Oh okay, I’ll check in the manufacturers forum as well then.

Thanks