Thanks for your possible help. I seem to have gotten past the potentiometer pixel issue.
I tried to combined two sketches that seems to be working okay individually, and it won’t load. It gets down to the very end with this error code.
exit status 1
expected ‘}’ at end of input
I have tried everything with } I have used up to three (which I’ve never seen more of) down to one with no luck.
If you could take a look and see if you can figure out why it seems to stop loading I would greatly appreciate it.
I Know I’ll have some code tweaking to do once it loads but Maybe I’m getting close to my ultimate solution.
Thank you so much for your time.
Cory
//
//Arduino code for Neopixel LED controller
// using a potentiometer and switch button
// (C) Ismail Uddin, 2015
// www.scienceexposure.com
#include <FastLED.h>
#include <Adafruit_GFX.h>
#include <Adafruit_NeoPixel.h>
#ifndef PSTR
#define PSTR // Make Arduino Due happy
#endif
#include <Adafruit_NeoPixel.h>
#define NUM_LEDS 31
#define NUM_PIXELS 31
#define DATA_PIN 5
Adafruit_NeoPixel strip = Adafruit_NeoPixel(31, DATA_PIN, NEO_GRB + NEO_KHZ800);
Adafruit_NeoPixel pixels = Adafruit_NeoPixel(NUM_PIXELS, DATA_PIN, NEO_GRB + NEO_KHZ800);
const byte potPin = A0;
const byte potPin2 = A2;
int litPixel = (6);
int val = 0;
int val_2 = 0;
int colorVal = 0;
int reading = 0;
int x;
int prevVal = 0;
int prevVal_2 = 0;
int switchPin = 13;
int Brightness = 0;
boolean lastBtn = LOW;
boolean NeopixelColor = false;
boolean lastButton = LOW;
uint32_t c_orange = strip.Color(248, 73, 3);
CRGB leds[NUM_LEDS];
void setup() {
// put your setup code here, to run once:
Serial.begin(9600);
strip.begin();
strip.show();
FastLED.show();
pinMode(switchPin, INPUT);
FastLED.addLeds<NEOPIXEL, DATA_PIN>(leds, NUM_LEDS);
pixels.begin(); // This initializes the NeoPixel library
}
void loop() {
// put your main code here, to run repeatedly:
//leds[25] = CRGB::Red;
//FastLED.show();
//delay(30);
//strip.setPixelColor(0-31,100,0,100);
//strip.setPixelColor(20,100,0,100);
int newPixel = map(analogRead(potPin2), 0, 1023, 20, 25);
pixels.setBrightness(10);
if (newPixel != litPixel)
{
for (int i = 21; i < NUM_PIXELS; i++)
for (int j = 0; j <21; j++)
{
if (i > newPixel && i < newPixel+6)
{
pixels.setPixelColor(i, pixels.Color(0,0, 255));
pixels.setPixelColor(j, pixels.Color(100,0, 100));
}
else
{
pixels.setPixelColor(i, pixels.Color(255, 255, 255));
}
}
pixels.show(); // This sends the updated pixel color to the hardware.
litPixel = newPixel;
reading = analogRead(potPin);
//reading = analogRead(potPin_2);
val = (reading/1024.0) * 10;
//val_2 = (reading/1024.0) * 25;
colorVal = (reading/1024.0) * 255;
if (digitalRead(switchPin) == HIGH && lastButton == LOW)
{
//delay(250); // Account for contact debounce
//NeopixelColor = !NeopixelColor;
}
if (NeopixelColor == false)
{
// Neopixel LED number code
strip.setBrightness(10);
if (val != prevVal)
//if (val_2 != prevVal_2)
{
for ( x = 0; x < val; x++)
//for ( x = 0; x < val_2; x++)
//for ( x = 10; x >= val; x--);
{
strip.setPixelColor(10 + x,CRGB::Blue); // increasing *
strip.setPixelColor(9 + x,CRGB::Blue); // increasing *
strip.setPixelColor(10 - x,CRGB::Blue); // decreasing
//strip.setPixelColor(9 + x,0); // increasing *
//strip.setPixelColor(11 - x,0); // decreasing
}
//for (x=val; x<22; x++)
//for (x=val_2; x<31; x++)
{
strip.setPixelColor(10 + x,100,0,100); // increasing Erasing *
strip.setPixelColor(10 - x,100,0,100); // decreasing Erasing
//strip.setPixelColor(10 + x,0,0,0); // increasing
//strip.setPixelColor(9 - x,0,0,0); // decreasing
//strip.show();
}
prevVal = val;
//prevVal_2 = val_2;
}
// else
{
strip.show();
}
}
else
{
// Neopixel Color code
for (x=0; x < prevVal; x++)
{
//strip.setPixelColor(x,colorVal,0,255-colorVal);
strip.show();
}
}
}