Powering Nema 23 + Sainsmart TB6560 Question

Hey guys I’m new to stepper motors and such. I’ve bought the easydriver and going to use it on another project but for this one I have a question.

I need to power a nema 23 stepper (maybe will be under 2lbs load) motor with a motor driver being the TB6560.

I want to hook up a power supply that is as small as possible, could I use something like this which is used for powering LED lights:

SUPERNIGHT AC 100-240V To DC 24V 3A 5.5x2.1mm DC Output Jack Power Supply

Or do I need to buy something like most people use I see in videos like this:

Dc 24v 15a Switching Power Supply Transformer Regulated

Thanks for all the help,

Travis