Evening all.
As per the subject, I’d like to power a string of 40 neopixels at 3.7v (LiPo)
If I read correctly, at full brightness, neopixels consume 60mA each (not sure if that’s at 5v or 3.7v though.)
So, 40 neopixels x 60mA /1000 = 2.4A
I am looking for a product that will allow me to charge the LiPo (with a USB/5V input) and simultaneously power the neopixels.
I already have this product: https://www.sparkfun.com/products/12711
Well, in truth, I have the much older version of this product that has 2 outputs (5V and SYS)
But I am not certain that this lipo usb charger will be able to provide 2.4A. The JST connectors imply to me (yes…an assumption) quite small guage wires that might not be able to carry more than 1A at best.
Is there a product that would meet the following criteria?
- 
Accept USB or another 5V input to charge a LiPo
 - 
Can charge a single 3.7 LiPo (perhaps as large as 6000mAH)
 - 
Provide at least 2.4A output to the circuit that it’s powering. I don’t mind if it outputs 5v or 3.7v. I can work with either
 
I don’t mind a small charge rate (even as low as 500mAh 100mAh is fine)
The application simply a light for my wood shed.
The light is probably only going to be turned on for 5 to 10 minutes every 2 days while I load up a basket and bring firewood into the house. At that use rate, I’m not going to be depleting the battery at any great rate.
Thanks for your consideration.
Be kind to eachother.
-Adrian