I have tried multiple times over multiple days to upload a ZIP file of my design. However, it is always stopping at step 2 of 3.
When on the step 2 page, https://www.batchpcb.com/zipnamer.php?o … d7c4, the only text showing is
Zip File Format Selector (Step 2 of 3)
X Max: 4.55 X Min: -0.0008
Y Max: 3.9009 Y Min: -0.0847
PCB Size: 18.13766848 inches square
Estimated price per board: $47.5 [$2.5/sq.in]
There are no buttons, links, or images. There’s definitely no indication of how to get to step 3.
The only HTML for the page is
<!-- left_navigation_eof //-->
    </table></td>
<!-- body_text //-->
    <td width="100%" valign="top"><table border="0" width="100%" cellspacing="0" cellpadding="0">
<tr><td class="pageHeading">Zip File Format Selector (Step 2 of 3)</td></tr>
<tr><td class="main">
<p style="text-align: center;"><b>X Max:</b> 4.55 <b>X Min:</b> -0.0008
<b>Y Max:</b> 3.9009 <b>Y Min:</b> -0.0847
<b>PCB Size:</b> 18.13766848 inches square
<b>Estimated price per board:</b> $47.5 [$2.5/sq.in]</p>
This looks like some script is running properly, but none of the surrounding page elements exist.
If it helps any, I have tried in Firefox 1.5.0.11 and IE 6.0.
Help resolving this would be very appreciated.