Problem on using MSP430 JTAG ISO in SBW mode

I use TI EZ430 with my target hardware.

I recently bought MSP430 JTAG ISO from Olimex since it claims that it can program the security fuse. But I could not succeed in using it in SBW mode. I made the following connections;

MSP430-JTAG-ISO pin-1(TDO/TDI) <—> Target Board (SBWTDIO)

MSP430-JTAG-ISO pin-7 (TCK) <—> Target Board (SBWTCK)

MSP430-JTAG-ISO pin-9 (GND) <—> Target Board (GND)

MSP430-JTAG-ISO pin-2 (VCC-Tool) <—> Target Board (VCC)

I use IAR kickstart V3.41A. The target processor is MSP430F2012.

I will highly appreciate any help.

I will also be happy to receive any note if anyone used MSP430 JTAG ISO with security fuse programming.

Best Regards,

Ahmet Arif Mumcu

Ankara-Turkey