Hi,
I bought a SparkFun 9DOF Razor IMU M0 to use it in a ROS project (on Ubuntu 18.04). The problem is with serial comunication: in Windows 10 I can upload the firmware and read serial comunication from serial monitor in the Arduino IDE.
When I plug the IMU in Ubuntu, first of all I cannot upload the firmware (for Ubuntu configuration I used the ROS guide in the link at the end of the post)
I cannot read the serial monitor too (Errore nell’apertura della porta seriale “/dev/ttyACM0”), so I cannot upload anything from Arduino IDE in Ubuntu.
The only way to read serial comunication in Ubuntu is using “socat stdio /dev/ttyACM0” from terminal.
Can you help me?
OS Linux: Ubuntu 18.04 LTS
OS Windows: 10 Home (ver 1809)
ROS distro: Melodic
ArduinoIDE (Ubuntu): 1.8.5 (from Ubuntu AppStore)
ArduinoIDE (Windows): 1.8.9 (from Windows Store)
ROS help: http://wiki.ros.org/razor_imu_9dof
Official help: https://learn.sparkfun.com/tutorials/9d … -guide/all
Info SparkFun Board: