I have a problem with mp3 card vs1053, I need to play a single song in loop mode with an arduino card, r3 but when you start the program every time you do the loop you notice the jump, how could you eliminate it?
Thank you.
I have a problem with mp3 card vs1053, I need to play a single song in loop mode with an arduino card, r3 but when you start the program every time you do the loop you notice the jump, how could you eliminate it?
Thank you.
Hello.
Which SparkFun product are you asking about? Can you tell us the SparkFun part number? Our part numbers are three letters, a dash and then 5 digits.
DEV-12660
I have a problem with mp3 card DEV-12660, I need to play a single song in loop mode with an arduino card, r3 but when you start the program every time you do the loop you notice the jump, how could you eliminate it?
Thank you.
I don’t believe you can unfortunately.
MP3 files are compressed and once the file stops playing, the VS1053 has to open the file, begin decompressing the file and then start playing. Because of that, there will be a slight pause between the end of the first play and beginning of the second. Sadly, this isn’t avoidable.