Hi,
I’m using OpenOcd 0.5.0 to debug and programming a fujitsu cortex m3 microcontroller and all work fine.
Now, i tried to upgrade to version 0.6.1 or 0.7.0, but i have some problems
The flash erase seems to work fine, but at the flash program i have following problems:
Info : Fujitsu MB9[AB]xxx: Chip Erase … (may take several seconds)
fm3 chip erase complete
Info : JTAG tap: mb9bfxx6.cpu tap/device found: 0x4ba00477 (mfg: 0x23b, part: 0xba00, ver: 0x4)
Error: mb9bfxx6.cpu – clearing lockup after double fault
target state: halted
target halted due to debug-request, current mode: Handler HardFault
xPSR: 0x01000003 pc: 0xfffffffe msp: 0xffffffd8
Polling target failed, GDB will be halted. Polling again in 100ms
Info : Fujitsu MB9B500: FLASH Write …
Error: timed out while waiting for target halted
Error: Error executing fm3 Flash programming algorithm
Error: error writing to flash at address 0x00000000 at offset 0x00000000
in procedure ‘flash’
make: *** [program] Error 1
To erase and program i’m using folliwing commands and .cfg files:
Commands:
specify OpenOCD configuration file (pick the one for your device)
OPENOCD_CFG = -f ./sk-fm3-176pmc-ethernet.cfg
#OPENOCD_CFG = -f ./openocd.cfg
specify OpenOCD flash programing commandos for FM3
OPENOCD_C += -c init
OPENOCD_C += -c jtag_khz 1000
OPENOCD_C += -c reset init
OPENOCD_C += -c verify_ircapture disable
OPENOCD_C += -c halt
OPENOCD_C += -c poll
OPENOCD_C += -c ‘fm3 chip_erase 0’
OPENOCD_C += -c reset halt
OPENOCD_C += -c ‘flash write_image $(PROJECT)_rom.bin 0x0 bin’
OPENOCD_C += -c reset run
OPENOCD_C += -c shutdown
program the FM3 internal flash memory with OpenOCD
program:
@echo “Flash Programming with OpenOCD …”
$(OPENOCD) $(OPENOCD_CFG) $(OPENOCD_C)
@echo “Flash Programming Finished.”
and the .cfg file used is
# MB9BF618T
interface ft2232
ft2232_vid_pid 0x0403 0x6010
ft2232_device_desc "Dual RS232"
ft2232_layout "oocdlink"
ft2232_latency 2
gdb_memory_map disable
if { [info exists CHIPNAME] } {
     set  _CHIPNAME $CHIPNAME
} else {
     set  _CHIPNAME mb9bfxx6
}
if { [info exists ENDIAN] } {
     set  _ENDIAN $ENDIAN
} else {
     set  _ENDIAN little
}
if { [info exists CPUTAPID ] } {
     set _CPUTAPID $CPUTAPID
} else {
     set _CPUTAPID 0x4ba00477
}
# delays on reset lines
jtag_ntrst_delay 500
# Fujitsu cortex-M3 reset configuration
reset_config trst_and_srst
jtag newtap $_CHIPNAME cpu -irlen 4 -ircapture 0x1 -irmask 0xf -expected-id $_CPUTAPID
set _TARGETNAME $_CHIPNAME.cpu
target create $_TARGETNAME cortex_m3 -endian $_ENDIAN -chain-position $_TARGETNAME
# Reset & Halt MCU, after debugger was connected
$_TARGETNAME configure -event gdb-attach {  
reset halt
}
$_TARGETNAME configure -event gdb-detach {
reset halt
}
# MB9BF618 has 128kB of SRAM on its main system bus 
$_TARGETNAME configure -work-area-phys 0x1FFF0000 -work-area-size 0x20000 -work-area-backup 0
# MB9BF618 has 1MB internal FLASH 
set _FLASHNAME $_CHIPNAME.flash
flash bank $_FLASHNAME fm3 0 0 0 0 $_TARGETNAME
# 4MHz / 6 = 666kHz, so use 500
#adapter_khz 500
adapter_khz 1000
# if srst is not fitted use SYSRESETREQ to
# perform a soft reset
cortex_m3 reset_config sysresetreq
What’s changed in new version?..I need to send different commands to perform that programming?
Best regards.
Roberto C.