Hi,
I’m trying to use OCD on a Intel XScale IXC1110 processor.
What have I understood is that XScale is ARM variant so it should work in some level with OCD right? When is the ‘full’ support coming?
I’m using JTAGkey and tried two different version of OpenOCD and neither of them worked. First was the version that came with the Amontec JTAGkey. There were some config files that I used but they gave me error: Error: jtag.c:1150 jtag_validate_chain(): Error validating JTAG scan chain, IR mismatch, scan returned 0x3F. Then I downloaded new version from http://www.yagarto.de/howto/openocd/index.html but it gave me same error.
I’m just wondering if there is any change of getting this to work with current version of OCD or is there still work to be done before OCD works ok with XScale?
Thanks.