Proper LoRaSerial USB Drivers Needed

I just got a Pair of LoRaSerial telemetry radios and would like to use them for my Facet Base/Rover setup. My Win7 PC, Win11 PC, Win7 Laptop and WinXP laptop ALL do not recognize them when I connect via the USB Port. My PC’s seem to recognoze them as Devices in the Windows Device Manager, but there is a ‘?’ beside the LoRa icon and a message saying there are missing Drivers. I read a post on here that had a link to some drivers for some other similar product that supposedly would work, but it didn’t. Most folks here seem to have them working, so I figure someone knows where I can get the correct drivers. Ideally, I’d like to use my small Win7 Home Laptop so I can monitor the RTCM Real Time Correction Messages sent from my Facet configured as a base station in the field. Thanks for any suggestions and help.

I believe that uses a SAMD21, we have drivers/guide for install here SAMD21 Mini/Dev Breakout Hookup Guide - SparkFun Learn

And also a win7-specific one here GitHub - sparkfun/samd_windows7_installer: Windows 7 installer package for SparkFun's SAMD21/SAMD51 based breakout boards

I’d give those a go, also try swapping usb cables/ports an re-try

Thank You for this. I did not come across it. I have not been able to get back to this, but I did get Win 11 to recognize the LoRa’a and was able to send messages back and forth using a serial term. This was good enough to jump right into the field and collect some data. They seemed to work fine for surveying with a Facet Base/Rover setup in open areas and in wooded areas over 600+ feet. Having some issues with getting a Fix , but that’s a Facet issue I think. Still trying to sort that out. I need a good way to mount the radios to a Facet and to make it more robust to attacks by the understory especially near swamps. It’s quite delicate.