I need to have three 14-Segment displays daisy chained but I am not sure how to remove the pull resistors. Per the instructions:
“As a general rule of thumb, disable all but one pair of pull-up resistors if multiple devices are connected to the bus. If you need to disconnect the pull up resistors they can be removed by cutting the traces on the corresponding jumpers highlighted below.”
Based on the schematic, am I supposed to remove one of the 4.7K resistors, either from the SDA or SCL? See the attached image. Am I supposed to ‘cut’ at point A and/or point B? Instead of ‘cutting’ (which I don’t like), may I remove the solders from pad X and/or pad Y? I know desoldering there may be a problem but just asking if technically possible.
Do all three have to be cut?
Thanks