Hi!
I have the MAX30101 & MAX32664 sensor https://www.sparkfun.com/products/15219
And am using the example code (Example1_config_BPM_Mode1) to read the heartrate.
This works (somewhat) and gives me expected results / detects the presence of a finger, but sometimes, if I don’t consistently keep my finger on the sensor, or if I leave it off for a while, or if my finger has been on the sensor for a little while, the sensor will appear to turn off and the LED on it will stop shining. I have to restart the Arduino to re-set up the sensor to get it to start working again. I still see the printed Serial output, but everything goes to 0, including status. The wiring is unfortunately a little convoluted now due to other things on the breadboard, but I don’t think it’s a wiring issue because consistently, if I don’t move it and it shuts off, if I restart it again it starts working, so it works in the ‘new position’.
Here’s what prints out on Serial Monitor:
Heartrate: 0
Confidence: 0
Oxygen: 0
Status: 0
Any ideas on why this is happening?
Thanks! I included the example code I’m using:
/*
 This example sketch gives you exactly what the SparkFun Pulse Oximiter and
 Heart Rate Monitor is designed to do: read heart rate and blood oxygen levels.
 This board requires I-squared-C connections but also connections to the reset
 and mfio pins. When using the device keep LIGHT and CONSISTENT pressure on the
 sensor. Otherwise you may crush the capillaries in your finger which results
 in bad or no results. A summary of the hardware connections are as follows: 
 SDA -> SDA
 SCL -> SCL
 RESET -> PIN 4
 MFIO -> PIN 5
 Author: Elias Santistevan
 Date: 8/2019
 SparkFun Electronics
 If you run into an error code check the following table to help diagnose your
 problem: 
 1 = Unavailable Command
 2 = Unavailable Function
 3 = Data Format Error
 4 = Input Value Error
 5 = Try Again
 255 = Error Unknown
*/
#include <SparkFun_Bio_Sensor_Hub_Library.h>
#include <Wire.h>
// Reset pin, MFIO pin
int resPin = 4;
int mfioPin = 5;
// Takes address, reset pin, and MFIO pin.
SparkFun_Bio_Sensor_Hub bioHub(resPin, mfioPin); 
bioData body;  
// ^^^^^^^^^
// What's this!? This is a type (like int, byte, long) unique to the SparkFun
// Pulse Oximeter and Heart Rate Monitor. Unlike those other types it holds
// specific information on your heartrate and blood oxygen levels. BioData is
// actually a specific kind of type, known as a "struct". 
// You can choose another variable name other than "body", like "blood", or
// "readings", but I chose "body". Using this "body" varible in the 
// following way gives us access to the following data: 
// body.heartrate  - Heartrate
// body.confidence - Confidence in the heartrate value
// body.oxygen     - Blood oxygen level
// body.status     - Has a finger been sensed?
void setup(){
  Serial.begin(115200);
  Wire.begin();
  int result = bioHub.begin();
  if (result == 0) // Zero errors!
    Serial.println("Sensor started!");
  else
    Serial.println("Could not communicate with the sensor!!!");
 
  Serial.println("Configuring Sensor...."); 
  int error = bioHub.configBpm(MODE_ONE); // Configuring just the BPM settings. 
  if(error == 0){ // Zero errors!
    Serial.println("Sensor configured.");
  }
  else {
    Serial.println("Error configuring sensor.");
    Serial.print("Error: "); 
    Serial.println(error); 
  }
  // Data lags a bit behind the sensor, if you're finger is on the sensor when
  // it's being configured this delay will give some time for the data to catch
  // up. 
  Serial.println("Loading up the buffer with data....");
  delay(4000); 
  
}
void loop(){
    // Information from the readBpm function will be saved to our "body"
    // variable.  
    body = bioHub.readBpm();
    Serial.print("Heartrate: ");
    Serial.println(body.heartRate); 
    Serial.print("Confidence: ");
    Serial.println(body.confidence); 
    Serial.print("Oxygen: ");
    Serial.println(body.oxygen); 
    Serial.print("Status: ");
    Serial.println(body.status); 
    // Slow it down or your heart rate will go up trying to keep up
    // with the flow of numbers
    delay(250); 
}