I am having issues with reading multiple differential voltages through the QUIIC ADS1015 and logging the data using the DataLogger IoT - 9DoF. I cut the jumper to remove the potentiometer, but I still only get differential voltage readings through the P0 N1 terminal configuration. I’ve noticed that if I have a differential configuration of P0 N3 for one and P1 N3 for a second, I will get a reading of the difference between the two voltages in the P0 N1 spot in the datalogger and a reading of 2047 or 2048 mV in the spots that correspond to P0 N1 and P1 N3 . I saw in the hookup guide that I may need a programmable comparator, but I’m not really sure how to go about that. Any suggestions?
Also, would I be able to use all 4 differential voltage configurations at once using only one QUIIC ADS1015 unit?