The Qwiic MP3 Trigger card is the perfects fit for the Wildlife Audio Deterrent Systems. The most recent problem is with the SD card receptacle. The SD card needs to be inserted from a location not on the trigger card. A micro SD card extension cable was used to locate the SD card receptacle on the exterior of the audio processor enclosure. The extension cable does not work with any of the Qwiic MP3 Trigger cards, but does work with all other micro SD card receptacles. Do i need a special extension cable to work with the Qwiic MP3 Tigger card?
Unfortunately, we do not carry this type of cable. So the cable could be an issue but I can’t verify that. Are you able to share detailed pictures of your setup?
The SD extension cable slides into the MP3 Trigger slot on the back side of the board. The other end is an extension slot for the SD card. The extension cable is about 5 inches long. I have tried two different makers of the cable and the MP3 trigger. Both cables do not read the SD card. Both cables do work when I use them in all other SD card slots on all other SD card readers.
There’s a ton of different ones on Amazon, for as cheap as they are, just order a few different ones and figure out what works best for your application.