Hey everyone, hopefully this is the right place to ask what is hopefully not a foolish question.
I’m working on a project to permanently install an Asus Tablet into a mount, and due to the dimensions of the mount, the orientation of the USB receptacle on the device won’t allow for connection of a cable (required for powering the device). To that end, I’m trying to re-work the I/O board of the device so I can turn the USB receptacle 90 degrees.
It all started nice and easy, opening the case and extracting the board was no real trouble. Once I got the board out, I realized extracting the receptacle off of it was going to be rather particular. I had never worked with anything SMD before, so I picked up the Simon SMD kit here to try my hand before going at the goal. The Simon kit proved pretty easy, and I did a bit of replacing components several times just to get a feel for it. That went well, so I went ahead and tried to extract the port from the Asus board. Long story short, that proved nowhere near as easy. The thermal sink that was the USB connector combined with presumably the lead-free solder was quite a nightmare for me. I was able to finally get it extracted without any harm coming to the unit.
Now, unfortunately, I have hit a snag. When I first started, I hopped on DigiKey and Mouser and found a few seemingly suitable receptacles. They were SMD and Vertical mount instead of the standard orientation mounts that it had. Perfect, I 'm thinking. Well, I went ahead and ordered a few of them, and to my dismay I find that all vertical mount Micro USB receptacles have a PCB footprint that is opposite pin orientation from my board. For the horizontal orientation, they have both “standard” and “reverse” - this being “standard”.
The obvious answer would just be “well flip the receptacle around, dummy”. Which would work in theory, but the way the PCB is laid out, there are a couple of small SMD components (looks like a capacitor and a couple resistors, maybe a diode) that are physically in the way if I turn the receptacle around.
So far, foiled! I was wondering if anyone had any suggestions as to a good approach here.
My board sans-extraction
http://i.imgur.com/fheysMa.jpgThe connectors I have tried have all been oriented like this guy