Dear all,
as of today I have a Red Board Qwiic https://www.sparkfun.com/products/15123 and plugged it up to my laptop using a USB cable that seemed to install nicely. When I Upload in Arduino 1.8.9 it uploads the files correcly and also does as intended (e.g. blinks LED when loading the BLINK example). But then, no matter which program I upload or from which USB Port, reading on-chip flash data fails:
avrdude: reading on-chip flash data:
Reading | avrdude: stk500_recv(): programmer is not responding
############avrdude: stk500_recv(): programmer is not responding
avr_read(): error reading address 0x0000
Full log below, thanks in advance ![]()
Arduino: 1.8.9 (Windows 10), Board: “Arduino/Genuino Uno”
C:\Program Files (x86)\Arduino\arduino-builder -dump-prefs -logger=machine -hardware C:\Program Files (x86)\Arduino\hardware -tools C:\Program Files (x86)\Arduino\tools-builder -tools C:\Program Files (x86)\Arduino\hardware\tools\avr -built-in-libraries C:\Program Files (x86)\Arduino\libraries -libraries \homedrive.htw-berlin.de\covariance\Eigene Dateien\Arduino\libraries -fqbn=arduino:avr:uno -vid-pid=1A86_7523 -ide-version=10809 -build-path C:\Users\covariance\AppData\Local\Temp\arduino_build_411642 -warnings=none -build-cache C:\Users\covariance\AppData\Local\Temp\arduino_cache_691765 -prefs=build.warn_data_percentage=75 -prefs=runtime.tools.arduinoOTA.path=C:\Program Files (x86)\Arduino\hardware\tools\avr -prefs=runtime.tools.arduinoOTA-1.2.1.path=C:\Program Files (x86)\Arduino\hardware\tools\avr -prefs=runtime.tools.avrdude.path=C:\Program Files (x86)\Arduino\hardware\tools\avr -prefs=runtime.tools.avrdude-6.3.0-arduino14.path=C:\Program Files (x86)\Arduino\hardware\tools\avr -prefs=runtime.tools.avr-gcc.path=C:\Program Files (x86)\Arduino\hardware\tools\avr -prefs=runtime.tools.avr-gcc-5.4.0-atmel3.6.1-arduino2.path=C:\Program Files (x86)\Arduino\hardware\tools\avr -verbose \homedrive.htw-berlin.de\covariance\Eigene Dateien\Arduino\sketch_jul19a\sketch_jul19a.ino
C:\Program Files (x86)\Arduino\arduino-builder -compile -logger=machine -hardware C:\Program Files (x86)\Arduino\hardware -tools C:\Program Files (x86)\Arduino\tools-builder -tools C:\Program Files (x86)\Arduino\hardware\tools\avr -built-in-libraries C:\Program Files (x86)\Arduino\libraries -libraries \homedrive.htw-berlin.de\covariance\Eigene Dateien\Arduino\libraries -fqbn=arduino:avr:uno -vid-pid=1A86_7523 -ide-version=10809 -build-path C:\Users\covariance\AppData\Local\Temp\arduino_build_411642 -warnings=none -build-cache C:\Users\covariance\AppData\Local\Temp\arduino_cache_691765 -prefs=build.warn_data_percentage=75 -prefs=runtime.tools.arduinoOTA.path=C:\Program Files (x86)\Arduino\hardware\tools\avr -prefs=runtime.tools.arduinoOTA-1.2.1.path=C:\Program Files (x86)\Arduino\hardware\tools\avr -prefs=runtime.tools.avrdude.path=C:\Program Files (x86)\Arduino\hardware\tools\avr -prefs=runtime.tools.avrdude-6.3.0-arduino14.path=C:\Program Files (x86)\Arduino\hardware\tools\avr -prefs=runtime.tools.avr-gcc.path=C:\Program Files (x86)\Arduino\hardware\tools\avr -prefs=runtime.tools.avr-gcc-5.4.0-atmel3.6.1-arduino2.path=C:\Program Files (x86)\Arduino\hardware\tools\avr -verbose \homedrive.htw-berlin.de\covariance\Eigene Dateien\Arduino\sketch_jul19a\sketch_jul19a.ino
Using board ‘uno’ from platform in folder: C:\Program Files (x86)\Arduino\hardware\arduino\avr
Using core ‘arduino’ from platform in folder: C:\Program Files (x86)\Arduino\hardware\arduino\avr
Detecting libraries used…
“C:\Program Files (x86)\Arduino\hardware\tools\avr/bin/avr-g++” -c -g -Os -w -std=gnu++11 -fpermissive -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics -Wno-error=narrowing -flto -w -x c++ -E -CC -mmcu=atmega328p -DF_CPU=16000000L -DARDUINO=10809 -DARDUINO_AVR_UNO -DARDUINO_ARCH_AVR “-IC:\Program Files (x86)\Arduino\hardware\arduino\avr\cores\arduino” “-IC:\Program Files (x86)\Arduino\hardware\arduino\avr\variants\standard” “C:\Users\covariance\AppData\Local\Temp\arduino_build_411642\sketch\sketch_jul19a.ino.cpp” -o nul
Generating function prototypes…
“C:\Program Files (x86)\Arduino\hardware\tools\avr/bin/avr-g++” -c -g -Os -w -std=gnu++11 -fpermissive -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics -Wno-error=narrowing -flto -w -x c++ -E -CC -mmcu=atmega328p -DF_CPU=16000000L -DARDUINO=10809 -DARDUINO_AVR_UNO -DARDUINO_ARCH_AVR “-IC:\Program Files (x86)\Arduino\hardware\arduino\avr\cores\arduino” “-IC:\Program Files (x86)\Arduino\hardware\arduino\avr\variants\standard” “C:\Users\covariance\AppData\Local\Temp\arduino_build_411642\sketch\sketch_jul19a.ino.cpp” -o “C:\Users\covariance\AppData\Local\Temp\arduino_build_411642\preproc\ctags_target_for_gcc_minus_e.cpp”
“C:\Program Files (x86)\Arduino\tools-builder\ctags\5.8-arduino11/ctags” -u --language-force=c++ -f - --c+±kinds=svpf --fields=KSTtzns --line-directives “C:\Users\covariance\AppData\Local\Temp\arduino_build_411642\preproc\ctags_target_for_gcc_minus_e.cpp”
Compiling sketch…
“C:\Program Files (x86)\Arduino\hardware\tools\avr/bin/avr-g++” -c -g -Os -w -std=gnu++11 -fpermissive -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics -Wno-error=narrowing -MMD -flto -mmcu=atmega328p -DF_CPU=16000000L -DARDUINO=10809 -DARDUINO_AVR_UNO -DARDUINO_ARCH_AVR “-IC:\Program Files (x86)\Arduino\hardware\arduino\avr\cores\arduino” “-IC:\Program Files (x86)\Arduino\hardware\arduino\avr\variants\standard” “C:\Users\covariance\AppData\Local\Temp\arduino_build_411642\sketch\sketch_jul19a.ino.cpp” -o “C:\Users\covariance\AppData\Local\Temp\arduino_build_411642\sketch\sketch_jul19a.ino.cpp.o”
Compiling libraries…
Compiling core…
Using precompiled core: C:\Users\covariance\AppData\Local\Temp\arduino_cache_691765\core\core_arduino_avr_uno_0c812875ac70eb4a9b385d8fb077f54c.a
Linking everything together…
“C:\Program Files (x86)\Arduino\hardware\tools\avr/bin/avr-gcc” -w -Os -g -flto -fuse-linker-plugin -Wl,–gc-sections -mmcu=atmega328p -o “C:\Users\covariance\AppData\Local\Temp\arduino_build_411642/sketch_jul19a.ino.elf” “C:\Users\covariance\AppData\Local\Temp\arduino_build_411642\sketch\sketch_jul19a.ino.cpp.o” “C:\Users\covariance\AppData\Local\Temp\arduino_build_411642/…\arduino_cache_691765\core\core_arduino_avr_uno_0c812875ac70eb4a9b385d8fb077f54c.a” “-LC:\Users\covariance\AppData\Local\Temp\arduino_build_411642” -lm
“C:\Program Files (x86)\Arduino\hardware\tools\avr/bin/avr-objcopy” -O ihex -j .eeprom --set-section-flags=.eeprom=alloc,load --no-change-warnings --change-section-lma .eeprom=0 “C:\Users\covariance\AppData\Local\Temp\arduino_build_411642/sketch_jul19a.ino.elf” “C:\Users\covariance\AppData\Local\Temp\arduino_build_411642/sketch_jul19a.ino.eep”
“C:\Program Files (x86)\Arduino\hardware\tools\avr/bin/avr-objcopy” -O ihex -R .eeprom “C:\Users\covariance\AppData\Local\Temp\arduino_build_411642/sketch_jul19a.ino.elf” “C:\Users\covariance\AppData\Local\Temp\arduino_build_411642/sketch_jul19a.ino.hex”
“C:\Program Files (x86)\Arduino\hardware\tools\avr/bin/avr-size” -A “C:\Users\covariance\AppData\Local\Temp\arduino_build_411642/sketch_jul19a.ino.elf”
Sketch uses 444 bytes (1%) of program storage space. Maximum is 32256 bytes.
Global variables use 9 bytes (0%) of dynamic memory, leaving 2039 bytes for local variables. Maximum is 2048 bytes.
C:\Program Files (x86)\Arduino\hardware\tools\avr/bin/avrdude -CC:\Program Files (x86)\Arduino\hardware\tools\avr/etc/avrdude.conf -v -patmega328p -carduino -PCOM4 -b115200 -D -Uflash:w:C:\Users\covariance\AppData\Local\Temp\arduino_build_411642/sketch_jul19a.ino.hex:i
avrdude: Version 6.3-20171130
Copyright (c) 2000-2005 Brian Dean, http://www.bdmicro.com/
Copyright (c) 2007-2014 Joerg Wunsch
System wide configuration file is “C:\Program Files (x86)\Arduino\hardware\tools\avr/etc/avrdude.conf”
Using Port : COM4
Using Programmer : arduino
Overriding Baud Rate : 115200
AVR Part : ATmega328P
Chip Erase delay : 9000 us
PAGEL : PD7
BS2 : PC2
RESET disposition : dedicated
RETRY pulse : SCK
serial program mode : yes
parallel program mode : yes
Timeout : 200
StabDelay : 100
CmdexeDelay : 25
SyncLoops : 32
ByteDelay : 0
PollIndex : 3
PollValue : 0x53
Memory Detail :
Block Poll Page Polled
Memory Type Mode Delay Size Indx Paged Size Size #Pages MinW MaxW ReadBack
eeprom 65 20 4 0 no 1024 4 0 3600 3600 0xff 0xff
flash 65 6 128 0 yes 32768 128 256 4500 4500 0xff 0xff
lfuse 0 0 0 0 no 1 0 0 4500 4500 0x00 0x00
hfuse 0 0 0 0 no 1 0 0 4500 4500 0x00 0x00
efuse 0 0 0 0 no 1 0 0 4500 4500 0x00 0x00
lock 0 0 0 0 no 1 0 0 4500 4500 0x00 0x00
calibration 0 0 0 0 no 1 0 0 0 0 0x00 0x00
signature 0 0 0 0 no 3 0 0 0 0 0x00 0x00
Programmer Type : Arduino
Description : Arduino
Hardware Version: 3
Firmware Version: 4.4
Vtarget : 0.3 V
Varef : 0.3 V
Oscillator : 28.800 kHz
SCK period : 3.3 us
avrdude: AVR device initialized and ready to accept instructions
Reading | ################################################## | 100% 0.00s
avrdude: Device signature = 0x1e950f (probably m328p)
avrdude: reading input file “C:\Users\covariance\AppData\Local\Temp\arduino_build_411642/sketch_jul19a.ino.hex”
avrdude: writing flash (444 bytes):
Writing | ################################################## | 100% 0.08s
avrdude: 444 bytes of flash written
avrdude: verifying flash memory against C:\Users\covariance\AppData\Local\Temp\arduino_build_411642/sketch_jul19a.ino.hex:
avrdude: load data flash data from input file C:\Users\covariance\AppData\Local\Temp\arduino_build_411642/sketch_jul19a.ino.hex:
avrdude: input file C:\Users\covariance\AppData\Local\Temp\arduino_build_411642/sketch_jul19a.ino.hex contains 444 bytes
avrdude: reading on-chip flash data:
Reading | avrdude: stk500_recv(): programmer is not responding
############avrdude: stk500_recv(): programmer is not responding
avr_read(): error reading address 0x0000
read operation not supported for memory “flash”
avrdude: failed to read all of flash memory, rc=-2
avrdude: stk500_recv(): programmer is not responding
avrdude done. Thank you.
the selected serial port
does not exist or your board is not connected