Attempting to upload a sketch to RedBoard Qwiic (DEV-15123) seems to succeed at first but ends with error:
OS: Windows 10
IDE: Arduino 1.8.19
Using Sparkfun AVR Boards 1.1.13
Using WCH Driver 3.7.2022.1
Sketch uploads without error on Arduino Uno, but even the “blink” sketch ends with an error on upload with the RedBoard Qwiic (though the LED still blinks as expected). I originally used the WCH driver that was automatically installed by Windows, but after noticing the error, I installed updated drivers – including FTDI (figured I would need it at some point anyway).
I’ve also attempted to uninstall everything and go back through the Hook-up Guide step-by-step, but the upload error persists. Thank you for any assistance you can offer.
Verbose Upload Output:
Arduino: 1.8.19 (Windows 10), Board: "SparkFun RedBoard"
Sketch uses 18606 bytes (57%) of program storage space. Maximum is 32256 bytes.
Global variables use 714 bytes (34%) of dynamic memory, leaving 1334 bytes for local variables. Maximum is 2048 bytes.
C:\Users\DLee\AppData\Local\Arduino15\packages\arduino\tools\avrdude\6.3.0-arduino17/bin/avrdude -CC:\Users\DLee\AppData\Local\Arduino15\packages\arduino\tools\avrdude\6.3.0-arduino17/etc/avrdude.conf -v -patmega328p -carduino -PCOM5 -b115200 -D -Uflash:w:C:\Users\DLee\AppData\Local\Temp\arduino_build_573535/DC2259.ino.hex:i
avrdude: Version 6.3-20190619
Copyright (c) 2000-2005 Brian Dean, http://www.bdmicro.com/
Copyright (c) 2007-2014 Joerg Wunsch
System wide configuration file is "C:\Users\DLee\AppData\Local\Arduino15\packages\arduino\tools\avrdude\6.3.0-arduino17/etc/avrdude.conf"
Using Port : COM5
Using Programmer : arduino
Overriding Baud Rate : 115200
AVR Part : ATmega328P
Chip Erase delay : 9000 us
PAGEL : PD7
BS2 : PC2
RESET disposition : dedicated
RETRY pulse : SCK
serial program mode : yes
parallel program mode : yes
Timeout : 200
StabDelay : 100
CmdexeDelay : 25
SyncLoops : 32
ByteDelay : 0
PollIndex : 3
PollValue : 0x53
Memory Detail :
Block Poll Page Polled
Memory Type Mode Delay Size Indx Paged Size Size #Pages MinW MaxW ReadBack
----------- ---- ----- ----- ---- ------ ------ ---- ------ ----- ----- ---------
eeprom 65 20 4 0 no 1024 4 0 3600 3600 0xff 0xff
flash 65 6 128 0 yes 32768 128 256 4500 4500 0xff 0xff
lfuse 0 0 0 0 no 1 0 0 4500 4500 0x00 0x00
hfuse 0 0 0 0 no 1 0 0 4500 4500 0x00 0x00
efuse 0 0 0 0 no 1 0 0 4500 4500 0x00 0x00
lock 0 0 0 0 no 1 0 0 4500 4500 0x00 0x00
calibration 0 0 0 0 no 1 0 0 0 0 0x00 0x00
signature 0 0 0 0 no 3 0 0 0 0 0x00 0x00
Programmer Type : Arduino
Description : Arduino
Hardware Version: 3
Firmware Version: 4.4
Vtarget : 0.3 V
Varef : 0.3 V
Oscillator : 28.800 kHz
SCK period : 3.3 us
avrdude: AVR device initialized and ready to accept instructions
Reading | ################################################## | 100% 0.00s
avrdude: Device signature = 0x1e950f (probably m328p)
avrdude: reading input file "C:\Users\DLee\AppData\Local\Temp\arduino_build_573535/DC2259.ino.hex"
avrdude: writing flash (18606 bytes):
Writing | #########avrdude: loadaddr(): (b) protocol error, expect=0x14, resp=0xfc
###avrdude: loadaddr(): (b) protocol error, expect=0x14, resp=0xfc
####################avrdude: loadaddr(): (b) protocol error, expect=0x14, resp=0xfc
#avrdude: loadaddr(): (b) protocol error, expect=0x14, resp=0xfc
avrdude: loadaddr(): (b) protocol error, expect=0x14, resp=0xfc
#######avrdude: loadaddr(): (b) protocol error, expect=0x14, resp=0xfc
##avrdude: loadaddr(): (b) protocol error, expect=0x14, resp=0xfc
###avrdude: loadaddr(): (b) protocol error, expect=0x14, resp=0xfc
##### | 100% 2.91s
avrdude: 18606 bytes of flash written
avrdude: verifying flash memory against C:\Users\DLee\AppData\Local\Temp\arduino_build_573535/DC2259.ino.hex:
avrdude: load data flash data from input file C:\Users\DLee\AppData\Local\Temp\arduino_build_573535/DC2259.ino.hex:
avrdude: input file C:\Users\DLee\AppData\Local\Temp\arduino_build_573535/DC2259.ino.hex contains 18606 bytes
avrdude: reading on-chip flash data:
Reading |
avrdude: stk500_paged_load(): (a) protocol error, expect=0x10, resp=0x69
avrdude: stk500_cmd(): programmer is out of sync
avr_read(): error reading address 0x0000
read operation not supported for memory "flash"
avrdude: failed to read all of flash memory, rc=-2
avrdude: stk500_disable(): protocol error, expect=0x14, resp=0x74
avrdude done. Thank you.
the selected serial port
does not exist or your board is not connected
This report would have more information with
"Show verbose output during compilation"
option enabled in File -> Preferences.