Hi there,
I’ve got four RedBoard QWIICs that I’m using with the SGP40 and BME280 QWIIC breakouts. Three of them work fine via USB 2.0 on my Ubuntu Server 22.04 system. The fourth, however, simply does not cooperate.
When I plug it into the Ubuntu computer’s USB 2.0 port, I get 1 TX blink, 1 less-bright RX blink immediately after, and then 2 Pin 13 LED blinks immediately after that. I have triple-checked and it is definitely blinking 13 TWICE and not three times. It will SOMETIMES start to connect if I hold the Reset button on the board until I see the RX LED blink and then immediately let go (the timing seems to be important). Sometimes, even on Windows 10, the Reset button trick doesn’t even work (like I said, the timing seems to be important). The BEST I have gotten from this sensor is the following (output from ```
‘sudo dmesg | tail --lines=20’
[867216.918592] usb 1-12.4.1: new full-speed USB device number 70 using xhci_hcd
I have already manually installed CH340 drivers as per the forum post recommended in the Linux section of the [[How To Install CH340 Drivers](https://learn.sparkfun.com/tutorials/how-to-install-ch340-drivers) instruction page. All three other boards do not display this behavior, although they are not perfectly identical (one of them has a differently-colored Pin 13 LED, blue instead of green). 
Before today, this was the DMESG response (same command as above):
[ 4098.578930] usb 3-1.1.1: new full-speed USB device number 13 using xhci_hcd
[ 4108.334715] usb 3-1.1.1: Device not responding to setup address.
[ 4118.170924] usb 3-1.1.1: Device not responding to setup address.
[ 4118.378527] usb 3-1.1.1: device not accepting address 13, error -71
I was able to connect to, reprogram, and read the Serial Monitor messages from this board on Win10 in the Arduino IDE. Please help! :cry:](https://learn.sparkfun.com/tutorials/how-to-install-ch340-drivers)