Reflashed the SD card for Jetbot AI Kit v2.0 but still cannot light up the Micro OLED

I was assembling the Jetbot SparkFun Jetbot AI Kit v2.0, and the problem appeared during the software setup.

After hooking up all the wires, the Micro OLED once lightened up and shows the information on it properly. However, I followed the old instruction and didn’t realize that the SD card is pre-flashed and I need to skip step 1. I got the Kingston CANVAS Go! Plus MicroSD card, so I flashed it with Jetbot Image v1.11.

I pluged the SD card back into the bot after reflashing it, but the screen still cannot light up.

Is there anything I can do to get the Jetbot back to normal?

Thank you a lot!

Lydia

This is an issue with how the bootloader works in the new version; you likely need to flash to an earlier image (v 1.10, that has an earlier version of Jetpack)…then, after completing the setup with the old version, pull out the card and put the newer image on it (v 1.11) and it should be good to go