Hello, I just setup the Jetbot kit and when booting it seems to get stuck at the very first bootloader screen showing the Nvidia logo without any errors. When checking the SD I found no errors with the card. I have seen others with the same error. Any help would be great.
Thanks for reaching out to us on this.
The best next step is to re-flash the SD card; be sure to use ‘belena etcher’ to flash the SD card with this image https://drive.google.com/file/d/1o08RPD … sp=sharing and start over.
Hope this helps, and happy sparking!
Welcome! I just as well got the same setup and had the exact same issue. Sad to say the Jetson Nano 4GB and 2GB are not the same and need their very own image. As you may guess the Jetbot 2.1 kit comes with the 2gb image. But very simple to fix! You will need to download the sparkfun_jetbot_v01-00.zip file and then reformat SD and flash the new image. Be sure to use this image since it has all the needed configuration. One you have this version all will work perfectly.
I wish that SparkFun could update their documentation about this issue.
Yes, it looks like I replied to my own message…the power of not having coffee. ![]()